AXIS#.MOTOR.ICONT

Description

This parameter is the motor continuous current.


  • This parameter is required to be configured for all motor types.

Context

For more information see Motor.

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type

Read/Write

Units

A

Range

0.1 to 500

Default Value

1

Data Type

Float
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
AXIS1.MOTOR.ICONT

500bh

10h

Unsigned32

-

1000:1

Read/Write

No

AXIS2.MOTOR.ICONT

510bh

10h

Unsigned32

-

1000:1

Read/Write

No

EtherNet/IP

Name

ID

Hex

Data Type

Access

Units

AXIS1.MOTOR.ICONT

6204

183C

Unsigned32

Read Only

-

AXIS2.MOTOR.ICONT

71740

1183

Unsigned32

Read Only

-

PROFINET

Parameter

PNU

Data Type

Access

Units

AXIS#.MOTOR.ICONT

6204

Float

Read Only

-